990-91397B-001

Safety Precautions

WARNING
Hazard of electric shock, explosion, or arc flash
  • Do not unpack the units before the time of installation.
  • Cover the units and store the units in a temperature controlled indoor environment free of conductive contaminants and humidity, where the units are protected from moisture until the time of start-up. Moisture inside the cabinet can create hazardous short circuits.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
WARNING
Hazard of dropping the cabinet
  • The cabinet must only be lifted and/or moved using the provided eye bolts as lifting points.
  • In case of hole deformation (ovalization) of the eye bolt, replace the eye bolt.
  • Use appropriate lifting equipment and lifting accessories (e.g. a crane with slings/chains) with a lifting capacity of minimum 300 kg (661 lbs).
  • Only use trained personnel to lift or move the cabinet.
  • Use appropriate personal protective equipment (PPE) such as helmets, gloves and safety shoes.
  • Follow all local regulations and guidelines for lifting equipment operations to ensure safety and compliance.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?