990-91397B-001

Storage

Storage temperature -25 °C to 55 °C (-13 °F to 131 °F)
Storage relative humidity 10 to 90% non-condensing
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?