Unpack the Cabinet
WARNING |
|---|
|
Tipping Hazard
The cabinet is top-heavy while on the pallet and may tip
over. Move and store with care. When moving the cabinet on the pallet,
secure the cabinet to the forklift/pallet truck and pay close attention
to the floor conditions and the balance of the cabinet.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
CAUTION |
|---|
|
Heavy load
Use adequate lifting/transport equipment.
Failure to follow these instructions can result in injury or equipment damage.
|
- Move the cabinet as close as possible to the final location with a pallet truck or a forklift before unpacking.
- Remove the packaging (cardboard, plastic, and foam corners).
- Unlock and open the front door.
- Remove the top gland plate. Store the top gland plate safely, it will be reinstalled during power cable connection.
- Remove the provided installation kit (marked (A) in the illustration) and the provided blank gland plate (marked (B) in the illustration) from the bottom of the cabinet. Save the installation kit and the blank gland plate for installation.
- Install the provided eye bolts from the installation kit:
WARNINGHazard of dropping the cabinet- The cabinet must only be lifted and/or moved using the provided eye bolts as lifting points.
- In case of hole deformation (ovalization) of the eye bolt, replace the eye bolt.
- Use appropriate lifting equipment and lifting accessories (e.g. a crane with slings/chains) with a lifting capacity of minimum 300 kg (661 lbs).
- Only use trained personnel to lift or move the cabinet.
- Use appropriate personal protective equipment (PPE) such as helmets, gloves and safety shoes.
- Follow all local regulations and guidelines for lifting equipment operations to ensure safety and compliance.
Failure to follow these instructions can result in death, serious injury, or equipment damage.- Install the four provided eye bolts in the top of the cabinet with the four provided M12 nuts. Torque the eye bolts to 67 Nm.
- Attach lifting equipment to the eye bolts. This will prevent the cabinet from tipping over when the cabinet is no longer attached to the pallet.
- Remove the four screws in the bottom of the cabinet.
- Close and lock the front door.
- Remove the left and right anchoring brackets. Reinstall
the screws.
WARNINGTip hazardThe cabinet is top-heavy and will tip over when no longer attached to the pallet. Move and store with care until it is time to anchor the cabinet to the floor and wall.Failure to follow these instructions can result in death, serious injury, or equipment damage. - Lift the cabinet down from the pallet using the eye bolts and appropriate lifting equipment.
- Lift the cabinet to the final installation location using the eye bolts and appropriate lifting equipment.
CAUTION