990-91264A-001

Connect the Power Cables in GVSBPSU60G-WP

Top Cable Entry System

Bottom Cable Entry System

  1. Connect the PE cables to the PE busbar.
  2. Perform one of the following:
    • For single mains: Connect the input cables from utility/mains.
    • For dual mains: Connect the bypass cables from utility/mains.
  3. Perform one of the following:
    • For single mains: Connect the UPS input cables.
    • For dual mains: Connect the UPS bypass cables.
  4. Connect the UPS output cables.
  5. Connect the load cables.
  6. Fasten the cables with cable ties to the cable reliefs as shown.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?