Prepare GVSBPSU60G-WP for Cables
![]() |
---|
hazard of electric shock, explosion, or arc flash
Do not drill or punch holes with the gland plates installed and do not drill or punch
holes in close proximity to the maintenance bypass panel.
Failure to follow these instructions will result in death or serious injury.
|
- Only for bottom cable entry system:
- Remove the cable relief in the bottom and install it in the top of the maintenance bypass panel.
- Remove the PE busbar in the top and install it in the bottom of the maintenance bypass panel.
- Remove the gland plates in the top or bottom of the maintenance bypass panel.
- Drill or punch holes for cables or conduits in the gland plates for signal cables
(A) and power cables (B).
DANGER
hazard of electric shock, explosion, or arc flashEnsure that there are no sharp edges that can damage the cables.Failure to follow these instructions will result in death or serious injury. - Install conduits (if applicable) and reinstall the gland plates.