990-91500B-001

Install the Seismic Anchoring (Option)

Use the optional seismic kit GVSOPT016 for this procedure.

  1. Mount the rear anchor assembly to the floor. Use appropriate hardware for the floor type – the hole diameter in the rear anchors is ø13 mm. Minimum requirement is M12 grade 8.8 hardware.

    Rear View

  2. Remove the bolts and remove the rear anchoring bracket. Save the bolts for adjacent installation of cabinets.

    Rear View

  3. Install the rear anchoring bracket on the UPS with the provided M8 bolts.

    Rear View of the UPS

  4. Push the UPS into position so the rear anchoring bracket connects to the rear anchors. The front anchoring bracket is installed in the final installation steps.

    Rear View of the UPS

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?