990-91500B-001

Connect the Signal Cables for Remote Alarm Panel (GVSOPT036) (Option)

  1. Connect the Class 2/SELV signal cables to the UPS output relays and route the signal cables out through the top of the UPS. Connect to terminal 1-8 in the remote alarm panel. See Connect the Signal Cables for details on routing the signal cables out of the UPS.
    Name Description Location on UPS Alarm text on UPS display Location on remote alarm panel Corresponding lamp on remote alarm panel
    OUT _1 (output relay 1) Preconfigured output relay Terminal J6617: 1,3 UPS in normal operation 1,2 UPS ONLINE
    OUT _2 (output relay 2) Preconfigured output relay Terminal J6617: 4,6 UPS common alarm 3,4 UPS General Alarm
    OUT _3 (output relay 3) Preconfigured output relay Terminal J6617: 7,9 UPS in battery operation 5,6 UPS on Battery
    OUT _4 (output relay 4) Preconfigured output relay Terminal J6617: 10,12 Battery voltage low 7,8 UPS Low Battery
  2. Remove the rear bottom gland plate and the rear bottom brush plate from the UPS.

    Front View of the UPS

  3. Perform one of the following:
    • For installation without conduits: Reinstall the brush plate.
    • For installation with conduits: Drill a hole in the gland plate for conduits, install conduits, and reinstall the gland plate.
  4. Connect the IMB signal cables to the terminal block TB3 and TB4 in the UPS and route the IMB signal cables out through the bottom of the UPS. Connect the IMB signal cables to terminal 9 and 10 in the remote alarm panel.

    Front View of the UPS

  5. Connect the provided signal cables 0W49487 and 0W49491 to the terminal block (11-14) in the remote alarm panel. Torque to 0.5-0.6 Nm (0.36-0.44 lb-ft / 4.42-5.31 lb-in). Route the signal cables out through the bottom of the remote alarm panel, and connect to the load equipment. The provided signal cables are 30 m (98.4 ft) long.

    Front View of the Remote Alarm Panel

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.