990-91500B-001

Installation Procedure

The UPS can be installed as a stand-alone UPS or with applicable options.

Overview of the UPS

Overview of the UPS with Options Installed

  1. Install the Seismic Anchoring (Option).
  2. Prepare for Installation.
  3. If a remote alarm panel (GVSOPT036) is part of your installation, follow the installation manual provided with this product to install it.
  4. If an output switch box (GVSOPT037) is part of your installation, follow the installation manual provided with this product to install it.
  5. Connect the Signal Cables.
  6. Connect the Signal Cables for EPO (Emergency Power Off).
  7. Only for installation with a remote alarm panel (GVSOPT036): Connect the Signal Cables for Remote Alarm Panel (GVSOPT036) (Option).
  8. Connect the External Communication Cables.
  9. Connect the Modbus Cables.
  10. Connect the Power Cables.
  11. Add Translated Safety Labels to Your Product.
  12. Final Installation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?