Connect the Power Cables in a 480 V System
For 4-wire systems:
-
Bonding jumper: Not connected
-
Technical/system earth: No local grounding electrode connected
For 3-wire systems:
-
Bonding jumper: Must be connected
-
Technical/system earth: A grounding electrode must be connected via the grounding electrode conductor.
- Only applicable to high impedance grounding systems:
- Remove the jumper cable between the PE busbar and the E terminal.
- Connect an external impedance between the PE busbar and E terminal according to NEC 2014 article 250.36.
- Connect the equipment grounding conductor/PE to the PE busbar.
- Connect the input cables.
- Only applicable to dual mains systems: Connect the bypass cables.
- Connect the output cables.
- Connect the DC cables to the battery+ and battery- busbars.
- For systems without internal backfeed disconnect device BF2: Fasten the provided plastic fasteners on the bypass cables in four places at 30 cm intervals. Adjust the fasteners to the bypass cables so they are fitted tightly together.
- For systems without internal backfeed disconnect device BF2: Fasten the provided plastic fasteners on the output cables in two places at 30 cm intervals. Adjust the fasteners to the output cables so they are fitted tightly together.