990-55777-001

Final Installation

  1. In the UPS, remove all debris and clean the cabling area. Remove the cardboard from the cabling area, and ensure that no cardboard pieces are left in the cabinet. Clean and vacuum the cabling area. See the UPS installation manual for details.
  2. Reinstall and close the inner doors on the UPS. See the UPS installation manual for details.
  3. Reinstall the transparent plate, the front cover, and the front door on the backfeed protection cabinet.
  4. Remove the plywood plates and the dust protection labels from the top of the backfeed protection cabinet and the UPS.

    Front View of the Backfeed Protection Cabinet and the UPS

  5. Follow the UPS installation manual to finish the installation of the UPS system.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?