990-55777-001

Position the Backfeed Protection Cabinet and the UPS without Seismic Anchoring

Use the top bracket TME73112 and installation bag number 2 for this procedure.

  1. Place the backfeed cabinet on the left side of the UPS and align the cabinets.
  2. Interconnect the backfeed protection cabinet and the UPS in the front with five screws as shown. The screws are provided in installation bag number 2.

    Front Left View of the Backfeed Protection Cabinet and the UPS

  3. Install the top bracket TME73112 between the backfeed protection cabinet and the UPS:
    1. Remove the plywood plate from the top of the UPS.

      Front View of the Backfeed Protection Cabinet and the UPS

    2. Install the top bracket TME73112 between the backfeed protection cabinet and the UPS.

      Front View of the Backfeed Protection Cabinet and the UPS

    3. Reinstall the plywood plate on the top of the UPS.

      Front View of the Backfeed Protection Cabinet and the UPS

  4. Push the backfeed protection cabinet and the UPS into position.
  5. Lower the front and rear leveling feet on the backfeed protection cabinet and the UPS with a wrench until they have full contact with the floor. The casters must not have contact with the floor. Use a bubble-leveler to check that the cabinets are level.
    NOTICE
    Risk of equipment damage
    Do not move the cabinets when the leveling feet have been lowered.
    Failure to follow these instructions can result in equipment damage.

    Front View of the Backfeed Protection Cabinet and the UPS

    NOTE: For installations with limited rear access, only lower the two front feet of each cabinet.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?