990-55777-001

Install the Seismic Anchoring and Position the Backfeed Protection Cabinet and the UPS

Use the optional seismic anchoring kit GVXLOPT002, the saved transportation brackets from the unpacking of the backfeed protection cabinet, the top bracket TME73112, and installation bag number 1 and 2 for this procedure.

DANGER
hazard of electric shock, explosion, or arc flash
Cover the front of the UPS with a plastic sheet while making anchoring holes to prevent dust or other conductive particles from entering the cabinet.
Failure to follow these instructions will result in death or serious injury.
WARNING
hazard of tilting
All rear and front seismic anchoring brackets must be installed.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  1. Cover the front of the UPS with a plastic sheet (marked (A) in the illustration) to protect against dust from drilling in the floor. Fasten the plastic sheet to the UPS with tape or similar to create a seal. The packaging bag can be cut and reused for the plastic sheet.

    Front View of the UPS

  2. Place the rear seismic anchoring brackets in the final installation area. The rear seismic anchoring brackets were removed from the UPS and the backfeed protection cabinet during unpacking of the cabinets.
  3. Connect the rear anchoring brackets for the UPS and the backfeed protection cabinet with the interconnection plate (marked (C) in the illustration). Use the screws provided in installation bag number 1. Mark the 14 anchoring holes in the rear seismic anchoring bracket assembly on the floor.

    Front View

  4. Drill the 14 anchoring holes according to national and local requirements.
  5. Remove the interconnection plate (marked (C) in the illustration) from the rear seismic anchoring brackets.
  6. Mount the rear seismic anchoring brackets to the floor. Use appropriate hardware for the floor type – the hole diameter in the rear seismic anchoring brackets is ø16 mm. Minimum requirement is M12 strength grade 8.8 hardware (not provided).
  7. Use a bubble-leveler to ensure that the rear seismic anchoring brackets are level. Use leveling shims if necessary.
  8. Push the UPS and the backfeed protection cabinet into position against the rear seismic anchoring brackets - the cabinets will connect to the conic outcroppings on the rear seismic anchoring brackets.
    CAUTION
    Risk of equipment damage
    When pushing the UPS into position, push on the frame to avoid damaging the signal cables/plates.
    Failure to follow these instructions can result in injury or equipment damage.

    Front View of the Backfeed Protection Cabinet and the UPS

  9. Fasten the cabinets to the rear seismic anchoring brackets by tightening the bolts on the front of the cabinets. Torque to 50 Nm.

    Front View of the Backfeed Protection Cabinet and the UPS

  10. Lower the two front feet on the UPS and the backfeed protection cabinet until the feet have full contact with the floor – use a bubble-leveler to ensure that the cabinets are level.
    NOTICE
    Risk of equipment damage
    Do not move the cabinets when the leveling feet have been lowered.
    Failure to follow these instructions can result in equipment damage.

    Front View of the Backfeed Protection Cabinet and the UPS

  11. Interconnect the backfeed protection cabinet and the UPS in the front with five screws as shown. The screws are provided in installation bag number 2.

    Front Left View of the Backfeed Protection Cabinet and the UPS

  12. Install the top bracket TME73112 between the backfeed protection cabinet and the UPS:
    1. Remove the plywood plate from the top of the UPS.

      Front View of the Backfeed Protection Cabinet and the UPS

    2. Install the top bracket TME73112 between the backfeed protection cabinet and the UPS.

      Front View of the Backfeed Protection Cabinet and the UPS

    3. Reinstall the plywood plate on the top of the UPS.

      Front View of the Backfeed Protection Cabinet and the UPS

  13. Remove the eight M8x30 screws from the front of the UPS. Remove the six M8x30 screws from the front of the backfeed protection cabinet. Save the screws as they are reused for the front seismic anchoring brackets.

    Front View of the Backfeed Protection Cabinet and the UPS

  14. Install the front seismic anchoring bracket on the backfeed protection cabinet with two M8x30 screws. Install the front seismic anchoring bracket on the UPS with two M8x30 screws.

    Front View of the Backfeed Protection Cabinet and the UPS

  15. Mark the 14 hole locations on the floor.

    Front View of the Backfeed Protection Cabinet and the UPS

  16. Remove the front anchoring brackets from the backfeed protection cabinet and the UPS. Secure the plastic sheet against the UPS with tape to create a seal.
    NOTE: The plastic sheet must be tight against the frame to protect the power modules from dust when drilling holes in the floor.
  17. Drill the 14 anchoring holes according to national and local requirements.
  18. Remove the plastic sheet from the front of the UPS.
  19. Reinstall the front seismic anchoring bracket on the backfeed protection cabinet with the six reused M8x30 screws. Reinstall the front seismic anchoring bracket on the UPS with the eight reused M8x30 screws.

    Front View of the Backfeed Protection Cabinet and the UPS

  20. Mount the front seismic anchoring brackets to the floor. Use appropriate hardware for the floor type – the hole diameter in the front seismic anchoring brackets is ø16 mm. Minimum requirement is M12 strength grade 8.8 hardware (not provided).

    Front View of the Backfeed Protection Cabinet and the UPS

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?