990-55777-001

Installation Procedure

Single Mains

Dual Mains

  1. Prepare the Backfeed Protection Cabinet and the UPS for Installation.
  2. Perform one of the following:
  3. Install Interconnection Busbars and Power Cables in the Backfeed Protection Cabinet and the UPS (380/400/415 V).
  4. Connect the Backfeed Signal Cable Between the Backfeed Protection Cabinet and the UPS.
  5. Add Translated Safety Labels to Your Product.
  6. Final Installation.
  7. Follow the UPS installation manual and other auxiliary product installation manuals to connect relevant signal cables and external communication cables in the UPS, and to finish the installation of the UPS system.
For moving or decommissioning the backfeed protection cabinet after installation has been completed, please see Decommission or Move the Backfeed Protection Cabinet to a New Location.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?