Command interface
Address | Register | Action | Size | Type | Units | Description |
---|---|---|---|---|---|---|
0x1482 |
5251 |
W |
1 |
UInt16 |
- |
Requested command |
0x1483 |
5252 |
W |
1 |
UInt16 |
- |
Reserved for future use |
0x1484 - 0x14FE |
5253 - 5375 |
W |
1 |
UInt16 |
- |
Command parameter 001 -123 |
0x14FF |
5376 |
R/W |
1 |
UInt16 |
- |
Command status |
0x1500 |
5377 |
R/W |
1 |
UInt16 |
- |
Command result codes:
|