DOCA0148EN-07

Firmware Version 003.012.002

New Features

Added MicroLogic Xi control units. A MicroLogic Xi is a control unit without Bluetooth Low Energy (BLE) communication.

Bugs Fixed

Time synchronization of IFM interface with IFE server did not happen when the IFE server was in Daylight Saving mode.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.