DOCA0148EN-07

Firmware Version 003.009.010

New Features

The following maintenance features have been added and are available with a MicroLogic X control unit with firmware version 003.011.000 or later:

  • New events for contact wear ratio.

  • New events for type of preventive maintenance to be performed.

Access has been added through Modbus registers to the following data for MasterPacT MTZ circuit breakers:

  • Average peak current demand.

  • Minimum and maximum values of real-time measurements.

  • Energy per phase values.

  • Main settings of the active setting group of current protection functions.

NOTE: The configuration of the connection to EcoStruxure Facility Expert is not available now. You can use Enerlin'X COM'X energy servers to configure the connection to EcoStruxure Facility Expert.

Bugs Fixed

The following bugs are fixed:

  • IFE server lost its clock master status when SNTP server did not answer.

  • IFE server restarted when discovery packet from Satchwell Sigma BMS platform was received.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?