DOCA0148EN-07

Firmware Version 003.006.011

New Features

The following features are added:

  • Access has been added through Modbus registers to the trip cause data for MasterPacT MTZ circuit breakers.

  • Support of alpha-numeric passwords for IFE webpages.

  • LV434002: Added support for the internal battery that maintains the date and time settings of the real-time clock (RTC) during a power loss.

  • Compatibility with ULP cables up to 20 m (65 ft) in length.

  • Alarm support for the MicroLogic P and H advanced protection settings, allowing an alarm email to be sent.

  • Discovery from IFE webpages of devices equipped with non-communicating trip units, through BCM or BSCM module (For example, ComPacT NSX non-communicating MicroLogic with BSCM module), for device status display only.

  • Compatibility with new MicroLogic 7 trip units for ComPacT NSX circuit breakers.

  • Integration of Acti9 Smartlink SI D as a remote device.

  • Modbus end-of-line termination default value in webpage for easier default configuration.

NOTE: The Schneider Electric automatic email profile is not available now. You have to use your own SMTP server.

Bugs Fixed

The following bugs are fixed:

  • FTP server could not be enabled in Italian language.

  • BCM firmware update was not performed when IFE server closed connection in DHCP mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?