DOCA0148EN-06

Firmware Version 003.010.005

New Features

Access has been added through Modbus registers to the following data for MasterPacT MTZ circuit breakers:

  • IDMTL protection trip

  • Over/Under frequency trip

  • Directional overcurrent trip

  • Discrepancy between display and MicroLogic

Bugs Fixed

The following bugs are fixed:

  • Modbus TCP communication was lost due to serial driver issue.

  • When IP Filtering was enabled as Read only, the Modbus function Scattered read was blocked.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?