DOCA0148EN-04

IFE Switchboard Server

When an intelligent modular unit (IMU) contains a circuit breaker equipped with a communicating MicroLogic trip unit, the IFE Ethernet switchboard server (IFE server) enables the IMU to be connected to an Ethernet network. Each circuit breaker has its own IFE server and a corresponding IP address.

The IFE server with part number LV434002 or LV434011 is an Ethernet interface for the circuit breaker in the IMU and a server for Modbus-SL (serial line) connected devices.

NOTE: The IFE server with part number LV434002 completely replaces the IFE server with part number LV434011. The part number LV434002 comes with the real time clock (RTC) feature and allows ULP connections up to 20 m (65.6 ft) with the MasterPact MTZ circuit breakers (LV434011 had a theoretical limitation of 5 m (16.4 ft) over the life of the IFE server).

The IFE server is compatible with the following ranges of circuit breakers:

  • MasterPact MTZ circuit breakers

  • MasterPact NT/NW circuit breakers

  • ComPact NS circuit breakers

  • ComPacT NSX circuit breakers

  • PowerPact P- and R-frame circuit breakers

  • PowerPacT H-, J-, and L-frame circuit breakers

NOTE: The information related to the new generation of ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers in this document applies to ComPact NSX and PowerPact H-, J-, and L-frame circuit breakers also. The exceptions are mentioned wherever applicable.
QR code for this page

Was this helpful?