VIGED310023EN-07

Dimensions

Device dimensions and cut-out for flush mount is illustrated in the following figure:

NOTE: All dimensions are measured in mm (in).

Observe the correct distances between devices for flush-mounting as per the following figure:

NOTE: All dimensions are measured in mm (in).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.