VIGED310023EN-07

Secure boot

Secure boot is a security feature built to ensures that only trusted and authenticated software is allowed to run during the system startup process.

  • Secure boot verifies the digital signatures of firmware drivers, bootloaders, and operating system components before executing them. It allows only software signed with trusted keys to run.

  • Secure boot blocks unauthorized or malicious code at the firmware level and helps prevent rootkits and pre-boot malware attacks.

Signed firmware update

Signed firmware update is a security mechanism which ensures that only verified and authorized firmware updates are installed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.