VIGED310023EN-07

Configuring the I/O configuration parameters

Configure the temperature sensor, relay, transformer relay and Insulation alarm ack relay parameters using the I/O Configuration screen.

To configure the I/O configuration parameters:

  1. Select the I/O Configuration folder to open the dialog showing the list of parameters.
  2. Choose the parameters you need to modify and select Edit.

    Parameters

    Options

    Description

    Temperature Sensor

    Normally open

    Normally closed

    Select the contact type for the temperature sensor to control injection exclusion.

    Relay

    Standard connection

    failsafe

    Choose the relay mode based on insulation monitoring requirements.

    Transformer Relay

    Standard connection

    failsafe

    Set the relay mode to monitor transformer insulation.

    Insulation Alarm Ack Relay

    Off

    On

    Turn alarm acknowledgment on or off.

  3. Select OK, and then select Send to save your changes to the device.
    NOTE: When changes are not saved to the device, the status bar on the bottom left screen shows Download Incomplete.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.