Configuring network parameters
- Navigate to .
- Modify the parameters value as per the following table:NOTE: Use the contextual menu buttons to modify the parameters value.
Parameter Allowed Values Default Value Description App -
Power C.
-
Control C
Power C
-
Select Power C for industrial or marine applications that contain power loads and power electronics such as speed drives, inverters, or rectifiers.
-
Select Control C for auxiliary control circuits used to drive power systems which contain sensitive loads such as PLCs, IOs, or sensors.
Filtering -
4s
-
40s
-
400s
40s
Select the filtering time depending on the application. NOTE: This value selection is restricted depending on the App value selection.Locating -
OFF
-
Prev.Al.
-
Alarm
-
IFL
Alarm
-
Select Alarm if boost mode is required in case of active insulation alarm and Insulation resistance is less than 2 KΩ (if using XD312 as fault locator).
-
Select Prev.Al if boost mode is required in case of active preventive insulation alarm and Insulation resistance is less than 50 KΩ (if using XD312H as fault locator).
-
Select IFL if boost mode is required in case of active preventive insulation alarm and Insulation resistance is less than 2 KΩ (if using IFL12, IFL12MC, IFL12LMC, IFL12MCT, and IFL12LMCT as fault locator).
NOTE:-
If you select Prev.Al., you need to select the preventive alarm threshold.
-
This value selection is restricted depending on the App value selection.
V.Adapt -
None
-
VA2
-
PHT1000
-
HV1700
None
Select the adaptor if the network voltage is greater than the rated network voltage of the device. NOTE: This value selection is restricted depending on the App value selection.Frequency -
50 Hz
-
DC
-
400 Hz
-
60 Hz
50 Hz
Select the rated frequency of the monitored power system. NOTE: This value selection is restricted depending on the App value selection.HRG -
OFF
-
0.1....2 MΩ
OFF
-
Select OFF when no grounding resistance is connected.
-
Select the value of the neutral grounding resistance, which is connected to the device.
-