7EN02-0417-02

About this guide

This guide explains about the commissioning procedure of Vigilohm IM400 / IM400L.

Throughout this guide, the term “device” refers to Vigilohm IM400 / IM400L. All differences between the models, such as a feature specific to one model, are indicated with the appropriate model number or description.

For detailed installation and operating instructions, including safety messaging, read the device instruction sheets and user manual.

The following table is profiled. Ensure care while modifying the contents.

Document Reference

Title Number
Instruction Sheet: Vigilohm IM400 / IM400L S1B90076
User Manual: Vigilohm IM400 / IM400L DOCA0049EN
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?