7EN02-0417-02

Setting date and time

On first power up, set the date and time. Setting date and time ensures proper timestamps for the logs and trends.
  1. Turn on the power supply.

    Auto-test begins in the device. Wait for 10 seconds for auto test to complete.

    • If auto-test passes, the INSULATION screen displays a resistance value. An example INSULATION screen is:

    • If auto-test fails, an error code is displayed.

  2. Press the flashing button.
    NOTE: The clock icon flashes to show that date and time needs to be set.

    The DATE/TIME screen displays.

  3. Set the date and time using the contextual menu buttons and .
  4. Press button to save the date and time.

    A message Saved displays.

    The Insulation screen displays a resistance value. An example INSULATION screen is:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?