Event Definition

Definition

An event is a change in state of digital data, or any incident detected by the MicroLogic X control unit, EIFE Ethernet interface, or IO modules.

Events are time stamped and logged in the event history of each module.

Events are categorized according to a level of severity:

  • High: urgent corrective action is required.

  • Medium: corrective action needs to be scheduled.

  • Low: for information only.

All high and medium severity events generate an alarm and a pop-up notification screen on the MicroLogic X control unit display screen.

Low severity events are information-type events. They can be consulted as follows:

  • With EcoStruxure Power Commission software.

  • With EcoStruxure Power Device app

Alarms and trips are events that require specific attention from the user:

  • A trip is a high severity event generated when the circuit breaker trips.

  • An alarm is an event with medium or high severity.

The information in this chapter is valid for events detected by the MicroLogic X control unit. Refer to the following documents for events detected by the EIFE Ethernet interface, or by IO modules:

Maintenance Events

Maintenance events are events that have an impact on the health state of the circuit breaker. They are notified by the service LED in addition to generating a medium or high severity event.

  • Orange service LED: medium severity detected alarm that requires non-urgent maintenance action.

  • Red service LED: high severity detected alarm that requires immediate maintenance action.

Management of Events by MicroLogic X Control Unit

The following diagram gives an overview of how events are managed by the MicroLogic X control unit.

Event Time Stamping

Each event is time stamped with the date and time of the MicroLogic X internal clock.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?