DOCA0102EN-12

Event Notifications

Presentation

High severity events (including trips) and medium severity events are notified by a pop-up screen on the MicroLogic X control unit.

Trip events are notified by SDE1 standard fault-trip indication contact and SDE2 optional fault-trip indication contact.

In addition, events can be configured to be notified in the following ways:

  • By optional M2C module.

  • By optional IO module.

  • By email from IFE or EIFE Ethernet interface.

Pop-up Screen

All high and medium severity events generate a pop-up screen on the MicroLogic X display screen Pop-up Event Messages:

  • A red pop-up screen indicates a trip or high severity event, needing immediate attention.

  • An orange pop-up screen indicates a medium severity event, recommending action.

The following table presents the medium severity events, displayed in an orange pop-up screen, which have auto-acknowledgment mode. For more information, see auto-acknowledgement mode.

Code Event
0x03F5 (1013) Ir prealarm (I > 90% Ir)
0x6200 (25088) Ir start (I > 105% Ir)
0x050C (1292) Ig alarm
0x050D (1293) IΔn alarm
0x6321 (25377) IDMTL long time operate
0x6310 (25360) Undervoltage on 1 phase operate
0x632A (25386) Undervoltage on all 3 phases operate
0x6311 (25361) Overvoltage on 1 phase operate
0x632B (25387) Overvoltage on all 3 phases operate
0x6315 (25365) Underfrequency operate
0x6316 (25366) Overfrequency operate
0x6214 (25108) Reverse power start
0x6314 (25364) Reverse power operate
0x6323 (25379) FW directional overcurrent operate
0x6324 (25380) RV directional overcurrent operate
0x6332 (25394) IDMT GF operate

M2C Notifications

EcoStruxure Power Commission software can be used to assign the notification of a group of up to eight events or alarms to either of the two M2C outputs.

The M2C output remains on as long as one of the events assigned to it is active or held.

EcoStruxure Power Commission software also enables the status of the M2C outputs to be forced.

Forcing an M2C output generates the following events:

Code

Event

History

Severity

0x130B (4875)

M2C output 1 is forced

Operation

Low

0x130C (4876)

M2C output 2 is forced

Operation

Low

Recommended Actions

Forcing an M2C output generates the following events:

Code

Event

Recommended actions

0x130B (4875)

M2C output 1 is forced

Unforce output with EcoStruxure Power Commission software.

0x130C (4876)

M2C output 2 is forced

Unforce output with EcoStruxure Power Commission software.

IO Module Notifications

When an output of the IO module is not assigned to a pre-defined application, EcoStruxure Power Commission software can be used to assign the notification of:

  • A single event.

  • A group of up to eight events or alarms.

For more information, refer to EcoStruxure Power Commission Online Help.

When the IO module output is assigned to a group of alarms, the output remains on as long as one of the events assigned to it is active or held. The operating mode of the IO module output must be set as non-latching.

EcoStruxure Power Commission software also enables the status of IO module outputs to be forced.

Refer to Enerlin'X IO - Input/Output Application Module for One Circuit Breaker - User Guide.

Email Notification

IFE or EIFE webpages allow events to be selected for notification by email. The notification by email is not configured by default.

For more information, refer to the relevant document:

  • Enerlin'X EIFE - Embedded Ethernet Interface for One MasterPacT MTZ Drawout Circuit Breaker - User Guide

  • Enerlin'X IFE - Ethernet Interface for One Circuit Breaker - User Guide

  • Enerlin'X IFE - Ethernet Switchboard Server - User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.