PKR8059401

Replacement Parts

When ordering replacement or spare parts, include as much information as possible. In many cases, the part number of a new part can be obtained by identifying the old part. Always include the description of the part. Specify the rating, vertical section, and factory order number of the equipment in which the part is used.

Parts List

Description

Part Number

Standard/Optional

Quantity

5kV vacuum contactor

Refer to specific order bill of materials

Standard

1

Power fuses

Refer to specific order bill of materials

Standard

3

Control power fuses

Refer to specific order bill of materials

Standard

2

Control power fuse, 10A

FU-627

Standard

1

Current transformers

Refer to specific order bill of materials

Standard

3

Relay, 3-pole, 120 Vac coil

Refer to specific order bill of materials

Standard

1

Relay base, 3-pole

Refer to specific order bill of materials

Standard

1

Relay, 4-pole, 120 Vac coil

Refer to specific order bill of materials

Optional

1

Relay base, 4-pole

Refer to specific order bill of materials

Optional

1

Indicator light replacement bulb

PD-52PX4EN

Standard

3

Electronic protective relay

Refer to specific order bill of materials

Standard

1

NOTE: Refer to MotorSeT instruction bulletin BRU3897001 for replacement or spare parts related to the control system, for ATL using MotorSeT Advanced Motor Control System.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.