PKR8059401

Diagrams

Standard ATL — Typical Views Diagram

Typical Views — Standard ATL Motor Controller

Legend — Typical Views of Standard ATL Motor Controller Diagram

A

Lifting eyebolts (removable)

B

Viewing window

C

Protective relay or MotorSeT Advanced Control Keypad

D

Start/Stop pushbuttons

E

Low voltage section

F

Medium voltage section

G

Ground bar for disconnecting switch

H

Disconnector switch handle

I

Current transformers (CT)

J

Ground fault CT (optional)

K

Control power transformers

L

Disconnector shield

M

Disconnector switch

N

Power fuses

O

Wireway

P

Vacuum contactor

Q

Motor landing pads

R

Ground bus

Compact ATL — Typical Views Diagram

Typical View — Compact ATL Motor Controller

Legend — Typical Views of Compact ATL Motor Controller Diagram

A

Lifting eyebolts (removable)

B

Viewing window

C

Protective relay or MotorSeT Advanced Control Keypad

D

Start/Stop pushbuttons

E

Low voltage section

F

Medium voltage section

G

Disconnector switch handle

H

Ground bus

I

Incoming bus (optional)

J

Disconnector switch

K

Control power transformers

L

Current transformers

M

Power fuses

N

Motor landing pads

O

Vacuum contactor

P

Ground fault CT (optional)

Dual ATL — Typical Views Diagram

Typical View — Dual ATL Motor Controller

Legend — Typical Views of Dual ATL Motor Controller Diagram

A

Lifting eyebolts (removable)

B

Infrared viewing windows

C

Protective relay or MotorSeT Advanced Control Keypad

D

Low voltage section

E

Medium voltage section

F

Incoming bus (optional)

G

Voltage divider card

H

Disconnector switch handle

I

Voltage transformers (VT)

J

Disconnector switch

K

Power fuses

L

Vacuum contactor

M

Ground bus

N

Control power transformer

Typical ATL Schematic


Legend — Typical Connection Diagram

A

Mains voltage

B

Disconnector switch

C

Main contactor

D

Current transformers (150:5)

E

Motor

F

Voltage transformer

G

Test/Run selector switch

H

Hand/Auto/Off selector switch

I

Disconnector switch interlock

J

Remote start/stop

K

To overload relay trip contact

L

Customer terminals for fault indication

M

Overload reset pushbutton

N

Overload relay

O

Run indicator light

P

Fault indicator light

Typical ATL schematic when using MotorSeT Advanced Motor Control System

Typical Connection Diagram — S2–Controlled ATL

NOTE: In order to show all details of a typical connection diagram, the figure has been split into two separate drawings. The drawings connect with each other. Connectors are flagged with captions “a” to “c” (in lower case letters on white background).
A Disconnector switch E Ground fault CT
B Power fuses F AC motor, 4160 Vac, 3–phase
C Current transformers G Control power fuses
D Main contactor H Control transformer
A Operational controls
1 Plant Interface Module (PIM)
1a Digital inputs
1b Modbus
1c Relay outputs
1d Analog outputs
1e Fibre
2 I/O module
2a Analog inputs
2b Analog outputs
2c Digital inputs
2d Digital outputs
3 RTD module
3a RTD inputs
4 Communications module
4a Fieldbus
6 Bus
B Switchgear controls
5 Motor Control Module (MCM)
5a Mains
5b Fibre
5c I/O
5d Ground fault
5e Phase current
5f Line voltage
5g Load voltage
C Switchgear
7 Main contactor
8 Divider card
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.