Line Isolation Monitor (LIM)

Iso-Gard™ Series 6 Line Isolation Monitor (LIM)

Iso-Gard Series 6 LIM

The Iso-Gard Series 6, microprocessor-controlled, Line Isolation Monitor (LIM) is included as standard equipment in all Schneider Electric hospital isolation panels. The Iso-Gard Series 6 LIM incorporates automatic and manual self-test and self-calibration to reduce the frequency of required periodic testing. Microprocessor controlled circuitry for highest accuracy and stability. UL Component Recognized and CSA Classified. Additional information can be found in the Iso-Gard Series 6 Line Isolation Monitor (LIM) Catalog, Document Number 4805CT1301.

Catalog Number

Description

Additional Detail

IG6M

Series 6 Line Isolation Monitor Included with each interior, mounted on TRIM

4800IG6C

Connector terminal Included with each interior, factory mounted

4800IG6CBKTVM

Connector terminal Required when installing IG6M into older Square D Isolation Power Systems
Mounting Bracket
Feedback