NNZ9886700

Simplified 3D CAD Models

DANGER
hazard of electric shock, explosion, or arc flash
  • The 3D CAD model provided is to be used for reference only.
  • Always obtain the latest revision of the model prior to performing equipment design.
  • Do not modify the mechanical or electrical parts contained in the assembly models. Any modification in the final design will void the UL recognition and warranty.
  • The performance of this product is dependent on the design and application of the complete electrical distribution equipment.
  • The designer of the electrical distribution equipment must consider the proper application of the components into the equipment, including use, potential misuse, and failure modes.
  • The complete electrical distribution equipment must be tested per all applicable codes and standards.
  • Read and understand all the instructions contained in this and other associated user guides prior to performing equipment design or manufacturing.
  • Use only the Square-D EvoPacT circuit breaker cradle with Square-D EvoPacT circuit breakers.
  • Use only the Square-D EvoPacT auxiliary cradle with Square-D EvoPacT auxiliary drawers.
Failure to follow these instructions will result in death or serious injury.

Simplified 3D CAD models are available upon request to assist as a reference in design, however they should not be used for final design. The final design must be validated and tested. Contact the local Schneider Electric representative for further information on obtaining a model.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?