QGH1336303-06

Button functions in editing setup parameters

Mode Button Function
Setup menu

Flashing digit: To decrease the numeric value.

Flashing value: To view the previous value from the list.

Flashing decimal point: To move decimal point to left.

Flashing digit: To increase the numeric value.

Flashing value: To view the next value from the list.

Flashing decimal point: To move decimal point to right.

Long press: Press and hold for 2 seconds.

Flashing digit: To move the position of the cursor to left.

To select a parameter to edit the values.

To save the changes made to setup parameter.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?