QGH1336303-06

Energy

The meter provides uni-directional, 2-quadrant, Class 1 / Class 0.5 accurate energy metering.

The meter stores accumulated value of any one of the selected energy from active, reactive, or apparent energy in nonvolatile memory when Source 1 = Utility and Source 2 = Genset or DG.:

  • Delivered (Utility): kWh, kVARh, kVAh

  • Delivered (Alternate source): kWh, kVARh, kVAh

  • Total (Utility + Alternate source): kWh, kVARh, kVAh

NOTE: Alternate sources are not available for PM1140H models.

Applicable for METSEPM1130HCL5LVD

NOTE: Based on the energy scale selection, all the energy parameter values will reset when any of the energy parameter exceeds 99999.999.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?