Retrofit

NOTE: Applicable only for PM2220/PM2230 meter models
NOTE: Applicable only for PM2220R/PM2230R meter models

The retrofit communication mode in the meter provides you an option for configuring legacy data models to communicate with the new models. The retrofit register map selection can be configured using HMI.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?