Configuring Favorite Page

NOTE: Applicable only for PM2220/PM2230 meter models
NOTE: Applicable only for PM2220R/PM2230R meter models

The meter allows you to select 4 parameters and arrange them in required order to be displayed in favorite page. These parameters can be selected only through communication and are customer based requirements. Some parameter logs are of utmost importance and navigating to those parameters takes time. For ease of navigation and accessibility, the meter allows you to choose 4 parameters and lock the page for easy reading.

The default Favorite Page parameters are:

  • Aavg

  • PFavg

  • Ptot

  • E.Del

  1. Start ION Setup and connect to your meter.
  2. Open I/O Setup and select the required parameter you want to configure.
  3. Configure the parameter and click OK.
    Below is the list of associated parameters which can be configured:
    • Current Average (Iavg)

    • Voltage L-L average (Vavg)

    • Voltage L-N average (Vavg)

    • Active Power total (Wtot)

    • Reactive Power total (VARtot)

    • Apparent Power total (VAtot)

    • Power Factor Average (PFavg)

    • Frequency (F)

    • Active Energy – Del (Wh-Del)

    • Reactive Energy – Del (VARh-Del)

    • Apparent Energy - Del (VAh-Del)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?