Setting the rate
- Navigate to .
- Enter the setup password (default is “0”), then press OK.
- Navigate to .
- Move the cursor to point to or to modify, then press Edit.
- Move the cursor to point to or to modify, then press Edit.
- Modify the parameter as required, then press OK.
- Press up arrow and press Yes to save your changes.
- Press the up arrow to exit.
Parameter Values
Description
Label Rate1 / Rate2
Example: CO2 Emission, Energy Cost
You can edit the label using ION Setup Channel None, Active Del, Active Rec, Active Del + Rec, Reactive Del, Reactive Rec, Reactive Del + Rec, Apparent Del, Apparent Rec, Apparent Del + Rec Select a channel from the list. Factor per (k__h) 0.000 to 99999.999 You can edit the factor value between 0.000 to 99999.999. To configure the Rate using ION Setup, see the “PM2000 series meter” topic in the ION Setup online help or in the ION Setup device configuration guide, available for download at www.se.comwww.usa.siemens.com/pds.