Retrofit setting

The following settings are required to enable the Retrofit communication mode in the meter.
  1. Navigate to Maint > Setup.
  2. Enter the setup password (default is “0”), then press OK.
  3. Press Comm. The Serial Port screen appears.
  4. Press Edit to select the Accumulated parameter.
  5. Press - or + to scroll to Retrofit.
  6. Press OK to select the Retrofit configuration.
  7. Press ▲ to return to the setup screen.
    NOTE: The existing configuration will be lost when you make new selection, so a confirmation screen appears.
    • Press Yes to accept the changes and return to the Setup screen.

    • Press No to keep the existing configuration and return to the Setup screen.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?