Ethernet communications

The meter uses Modbus TCP and BACnet/IP protocols to communicate at data speeds up to 100 Mbps through its Ethernet communications port (if available).

The meter supports a maximum of 128 concurrent TCP/IP connections.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.