Binary Input objects

Your meter has a number of Binary Input objects that provide the status information from the meter’s I/O.

The following table lists the Binary Input (BI) objects available on the meter.

Object ID Object name Description
38416, 38417

Digital Input 1

Digital Input 2

Status of digital inputs 1 and 2:

  • 0 = on
  • 1 = off

NOTE: This information only applies if the digital input is configured as a status input.
38448, 38449

Digital Output 1

Digital Output 2

Status of digital outputs:

  • 0 = on
  • 1 = off

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.