Ethernet configuration

In order to use Ethernet communications, you must configure your device’s IP address; you must also configure the subnet and gateway information if required by your network.

You need to enter network information for any Ethernet servers used by the device.

NOTE: Contact your network system administrator for your IP address and other Ethernet network configuration values.

Configure your device’s Ethernet settings by using the display. Modify your meter’s Ethernet settings to those provided by your network system administrator before connecting the device to your local area network (LAN).

After the meter’s Ethernet port is configured and connected to the LAN, you can use ION Setup to configure other meter setup parameters.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.