Multi-state Input objects

Your meter has a number of Multi-state Input objects that provide information about the meter’s I/O and power system settings.

Meter configuration multi-state input objects

Object ID Object name Object name / description
2016

Power System Type

Power system configuration:

  • 0 = 1PH2W L-N
  • 1 = 1PH2W L-L
  • 2 = 1PH3W L-L with N
  • 3 = 3PH3W ungrounded delta
  • 4 = 3PH3W corner grounded delta
  • 5 = 3PH3W ungrounded wye
  • 6 = 3PH3W grounded wye
  • 7 = 3PH3W resistance grounded wye
  • 8 = 3PH4W center-tapped open delta
  • 9 = 3PH4W center-tapped delta
  • 10 = 3PH4W ungrounded wye
  • 11 = 3PH4W grounded wye
  • 12 = 3PH4W resistance grounded wye

2036

VT Connection Type

VT connection type:

  • 0 = Direct connect
  • 1 = Delta (2 VT)
  • 2 = Wye (3 VT)
  • 3 = L-N (1 VT)
  • 4 = L-L (1 VT)
  • 5 = L-L with N (2 VT)

3701

Demand Method - Power

Power demand method:

  • 0 = Thermal demand
  • 1 = Timed interval sliding block
  • 2 = Timed interval block
  • 3 = Timed interval rolling block
  • 4 = Input synchronized block
  • 5 = Input synchronized rolling block
  • 6 = Command synchronized block
  • 7 = Command synchronized rolling block
  • 8 = Clock synchronized block
  • 9 = Clock synchronized rolling block

3711

Demand Method - Current

Current demand method:

  • 0 = Thermal demand
  • 1 = Timed interval sliding block
  • 2 = Timed interval block
  • 3 = Timed interval rolling block
  • 4 = Input synchronized block
  • 5 = Input synchronized rolling block
  • 6 = Command synchronized block
  • 7 = Command synchronized rolling block
  • 8 = Clock synchronized block
  • 9 = Clock synchronized rolling block

3721

Demand Method - Input Metering

Input metering demand method:

  • 0 = Thermal demand
  • 1 = Timed interval sliding block
  • 2 = Timed interval block
  • 3 = Timed interval rolling block
  • 4 = Input synchronized block
  • 5 = Input synchronized rolling block
  • 6 = Command synchronized block
  • 7 = Command synchronized rolling block
  • 8 = Clock synchronized block
  • 9 = Clock synchronized rolling block

I/O multi-state input objects

The following table lists the Multi-state Input objects that provide information about meter’s I/O configuration.

Object ID Object name Description
7274, 7298

Digital Input 1 Mode

Digital Input 2 Mode

Digital input control mode

  • 0 = Normal (Alarm)
  • 1 = Demand Interval Sync Pulse
  • 2 = Multi-tariff Control

9673, 9681

Digital Output Mode 1

Digital Output Mode 2

Digital output 1 and 2 control mode

  • 0 = External
  • 1 = Demand Sync
  • 2 = Alarm
  • 3 = Energy

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.