80043-055-16

Reference Publications

Schneider Electric publications are available through your local Schneider Electric representative. These publications include device replacement procedures and listings of spare parts to make ordering and servicing of replacement parts quick and convenient. Any maintenance procedure or device not listed, such as an I-Line interior, is not customer serviceable.

Contact your local Schneider Electric representative for information at 1-888-778-2733 in the US, or at 1-800-565-6699 in Canada. Or, refer to the Technical Library at http://www.schneider-electric.us/ to obtain the appropriate publications.

For information about obtaining NEMA documents, write to:

National Electrical Manufacturers Association (NEMA)
Attention: Customer Service
1300 North 17th Street
Suite 1847
Rosslyn, VA 22209

Reference Publications

Other Reference Publications

Publication Number

General Instructions for Proper Installation, Operation, and Maintenance of Switchboards Rated 600 V or Less

NEMA Publication PB2.1

Application Guide for Ground Fault Protective Devices for Equipment

NEMA Publication PB2.2

Circuit Breakers

NEMA Publication AB-4

Enclosed and Miscellaneous Distribution Switches

NEMA Publication KS-1

Standard for Electrical Equipment Maintenance

NFPA 70B-2023

Damaged Breakers Bulletin

0600DB1103

Water Damaged Electrical Distribution and Control Equipment

0110DB0401R0711

Evaluating-Water Damaged-Electrical-Equipment-Guide

NEMA Publication GD 1-2019

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.