80043-055-16

Maintaining the Switchboard

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Inspect and perform preventive maintenance only on switchboards and equipment that has been de-energized and electrically isolated (unless otherwise specified). This minimizes the chance that accidental contact cannot be made with energized parts.
  • Follow safety-related work practices as described in NFPA 70E, Part II at all times.
Failure to follow these instructions will result in death or serious injury.

Periodic maintenance of the switchboard includes cleaning, lubrication, and exercising component parts. The interval between maintenance checks varies depending upon the amount of usage and environmental conditions of each installation. The maximum recommended inspection interval is one year. This definition for periodic maintenance applies throughout this manual, unless otherwise noted.

Always inspect the switchboard after a trip occurs. (Refer to Adverse Circumstances). Service bulletins for the various disconnecting and overcurrent devices mounted in the switchboard are available through your local Schneider Electric representative.

General Inspection and Cleaning

  1. Vacuum the switchboard interior to remove any dirt or dust deposits. Wipe all bus bars, insulators, cables, and other items with a clean, dry, lint-free cloth.

  2. Please refer to Moisture Contamination Avoidance and Mitigation if moisture, condensation build-up, or signs of any previous wetness are discovered.

    NOTICE
    Contamination Hazard
    • Do not use an air hose to blow out the switchboard. Dust can settle inside relays and overcurrent devices, causing overheating and improper operation.
    • Do not allow paint, chemicals, or petroleum-based solvents to contact plastics or insulating materials.
    Failure to follow these instructions can result in equipment damage.
  3. Inspect the switchboard for any signs of overheating. Discoloration and flaking of insulation or metal parts are indications of overheating.

    NOTE: If overheating occurs, be sure that all conditions that caused the overheating have been corrected. Loose or contaminated connections can cause overheating.
  4. Check for signs of rodent nesting in the switchboard. If required, use a good exterminating technique in the general area of the switchboard.

    NOTE: Do not place or use exterminating substances and chemicals inside the switchboard. Some products attract rodents.
  5. Carefully inspect all devices for any visibly worn-out, cracked, or missing parts.

  6. Manually open and close switches and circuit breakers several times to verify they are working properly.

  7. Verify that all key interlocks and door interlocking provisions are working properly.

Bus Bar Joints, Lug Terminations, and Insulating Materials

NOTE: Bus bar joints are maintenance-free. Do not retighten them after the pre-energizing checkout procedure is complete.
NOTICE
Plating damage
  • Do not sand or remove plating on any bus bar, splice bar, or terminal lug.
  • Damage to plating can result in overheating. Replace damaged part. Contact Schneider Electric Services at 1-888-778-2733 (US) or 1-800-565-6699 (Canada).
Failure to follow these instructions can result in equipment damage.
  1. Check all bus bar joints and terminal lugs for any pitting, corrosion, or discoloration resulting from high temperatures or subjection to high trip conditions. If any damage has occurred, replace the bus bars or lugs. If cleaning is required, use Lectra-Clean®, or similar type of cleaner.

    NOTE: Do not to apply chemicals while the bus bar joints or terminal lugs are inside the switchboard.
  2. Inspect all insulating materials. Before re-energizing the switchboard, replace insulators with any visible damage (such as cracks).

General Lubrication Information

For field maintenance re-lubrication of blade/jaw components in switches 600 V and below, use BG20 High Performance Synthetic Grease from Dow Corning (Schneider Electric catalog number SWLUB). This grease is applicable for the following switches:

  • Bolt-Loc

  • QMB Main and Branch

  • QMJ Branch

  • QMQB* Main and Branch

For bus/plug-on connections, use electric joint compound, Schneider Electric catalog number PJC7201.

For MasterPacT drawout connections, use only Schneider Electric catalog number S48899 Electric Joint Compound.

Automatic Transfer Switches

Consult the documentation provided by the manufacturer for all installation, operation, and maintenance instructions for these devices.

Bolt-Loc Bolted Pressure Contact Switch Maintenance, 800-4000 A

Refer to the Bolt-Loc switch installation and maintenance manual for complete information (manual is shipped with the switchboard). If the manual is not available, refer to Reference Publications, and contact your local Schneider Electric representative to obtain the appropriate manuals.

  1. Exercise the operating mechanism at least once a year to validate proper operation.

  2. The Bolt-Loc switch is shipped from the factory properly lubricated. Periodic cleaning and lubrication of the switch is required. The maintenance interval between lubrications depends on factors such as usage and ambient conditions. The maximum recommended maintenance interval is one year for current-carrying parts and five years for operating mechanisms.

    DANGER
    HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Always check line and load ends of the fuses for voltage before starting the replacement procedure. The Bolt-Loc switch can be part of a multiple source system in which the fuses can be energized when the Bolt-Loc switch is in the “open” position.
    Failure to follow these instructions will result in death or serious injury.
  3. To replace the fuse:

    1. Open the switch before opening the fuse door (see Type BP Bolt-Loc Fusible Switch).

      Type BP Bolt-Loc Fusible Switch

    2. Open the fuse door, releasing the interlock as described in the instructions on the door.
    3. Observe the switch blades to confirm the switch is “open.”
    4. Check the line and load ends of fuses for voltage using a properly rated voltage sensing device. No voltage should be present.
    5. Remove all fuses. Retain the hardware for reuse.

    6. Using a non-abrasive cleaner such as Lectra-Clean, made by CRC, wipe clean the fuse mounting pads on the switch and the terminals of each new fuse. Check the alignment of fuse terminals before installing new fuses.
      NOTE: Take care when using the Lectra-Clean so that it does not inadvertently contact other part.
    7. Install new fuses using the same hardware removed in Step e. Tighten to 21–30 lb-ft. (28–41 N•m).
  4. Close the fuse door, and check the fuse door interlock with the switch in the ON position. The fuse doors should not open using normal force.

Circuit Breakers

Schneider Electric circuit breakers are designed and manufactured as sealed units requiring minimal periodic maintenance.

Exercise circuit breakers at least once a year to validate proper operation. For general maintenance:

  1. Trip the circuit breaker by pushing the Push-To-Trip or “Open” button located on the face of the circuit breaker. Refer to the appropriate circuit breaker manual for the specific location of this button (see PowerPacT R-Frame Circuit Breaker).

  2. Manually open and close the circuit breaker two to three times.

    PowerPacT R-Frame Circuit Breaker

    NOTE: Schneider Electric instruction bulletin 0600IB1201, Field Testing and Maintenance Guide for Thermal-Magnetic and MicroLogic™ Electronic Trip Molded Case Circuit Breakers, provides more in-depth information.
    DANGER
    HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    • If adjusting circuit breaker settings, do not set the long-time trip rating at a higher ampacity than the rating of the bus bar or load cables it supplies; overheating can occur.
    • Before energizing the switchboard, fill all unused I-Line circuit breaker mounting spaces with blank fillers and/or extensions as listed in I-Line Blank Fillers and Extensions.
    Failure to follow these instructions will result in death or serious injury.

    Refer to individual circuit breaker instruction manuals shipped with the switchboard for additional maintenance information, such as changing rating plugs, sensor plugs, or adjustable settings and removing circuit breakers. If the instruction manual is not available, refer to Reference Publications for the appropriate number, or contact your local Schneider Electric representative.

    I-Line Blank Fillers and Extensions

    Item

    Height

    Catalog No.

    Branch Circuit Side

    Circuit Breaker Frame

    Blank Fillers

    1.50 in. (38 mm)
    4.50 in. (114 mm)

    HNM1BL
    HNM4BL

    Both Sides
    Both Sides

    Not applicable

    Blank Extensions

    1.50 in. (38 mm)
    4.50 in. (114 mm)
    1.50 in. (38 mm)
    4.50 in. (114 mm)

    HLW1BL
    HLW4BL
    HLN1BL
    HLN4BL

    Wide Side
    Wide Side

    Narrow Side
    Narrow Side

    All applications except PowerPacT H/J circuit breakers with MicroLogic trip unit 5/6.

    4.50 in. (114 mm)
    4.50 in. (114 mm)

    HLN4EBL
    HLW4EBL

    Narrow Side
    Wide Side

    Only PowerPacT H/J circuit breakers with MicroLogic trip unit 5/6.

    NOTICE
    Plug-On Connector DAMAGE
    • Do not remove the protective lubricant on the plug-on connectors.
    • If additional lubrication is required, apply a coating of electrical joint compound, catalog number PJC7201, to the contact surfaces of the plug-on connector.
    Failure to follow these instructions can result in equipment damage.
  3. A full function test kit, catalog number FFTK, is available from Schneider Electric to test PowerPacT M, P, and R circuit breakers equipped with MicroLogic trip units. It runs trip unit tests automatically, with prompts to the user for initial information. Test modules for each circuit breaker frame are used to store data necessary for automatic tests. Series B MicroLogic trip units require test module CBTMB, which is included in UTS3.

    A pocket tester, catalog number S434206, or UTA tester, catalog number STRV00910, are available from Schneider Electric to test PowerPacT H-, J-, and L-frame circuit breakers with MicroLogic trip units. These testers supply power to the MicroLogic trip units and allow for settings to be adjusted through the keypad located on the circuit breaker or through a PC using the USB interface.

    To test MasterPacT NW circuit breakers with MicroLogic trip units, use the fullfunction test set, catalog number S33595, or the hand-held test set, catalog number S33594, which are available from Schneider Electric.

    To test MasterPacT MTZ circuit breakers and control units, use EcoStruxure, which is available from Schneider Electric.

    NOTE: Tests can be conducted with a circuit breaker installed in the switchboard; circuit breaker removal is not required. The switchboard must be de-energized.

QMB/QMJ/QMQB Fusible Switches

NOTE: QMQB switches are available in Canada only.

Refer to the QMB/QMJ/QMQB instruction manual for complete maintenance information. If the instruction manual is not available, refer to Reference Publications of this manual for the appropriate number. Contact your local Schneider Electric representative to obtain the manual.

Switch Maintenance

  1. Periodically exercise the switch to validate proper operation. This period should not exceed one year.

  2. Check the cover interlock with the switch in the ON position. The cover should not open using normal hand force.

  3. Inspect the switch interior for any damaged or cracked parts, and replace as necessary.

  4. For fusible switch units, check the fuse mounting clips or bolted contact area for corrosion or discoloration (indicating overheating). Replace them if necessary.

  5. For additional maintenance instructions, see the label on the inside of the door.

Fuse Replacement (Fusible Switches Only)

  1. Turn the switch to the OFF position before opening the door.

    DANGER
    HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Always check line and load ends of the fuses for voltage before starting the fuse replacement procedure with a properly rated voltage sensing device.
    Failure to follow these instructions will result in death or serious injury.
  2. Observe the switch blades to confirm that the switch is in the OFF position.

  3. Using a properly rated voltage sensing device, verify that line and load ends of the fuse are not energized.

  4. Observe all hazard labels specifying the type of fuse to use. Do not substitute a non-current limiting fuse, or attempt in any way to defeat the rejection feature of the fuse clips furnished with the switch. Do not use renewable link fuses in Schneider Electric fusible switches.

    NOTICE
    fuse clip overheating
    Do not pry open or spread the fuse mounting clips. Doing so can cause a loose connection, resulting in overheating and nuisance fuse opening.
    Failure to follow these instructions can result in equipment damage.

Installing QMB/QMJ/QMQB Fusible Switches

NOTE: QMQB switches are available in Canada only.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Remove power for these sections before installing or removing QMB/QMJ/QMQB* switches.
  • Do not use a main as a branch unit or a branch as a main.
  • All unused spaces must be filled with blank fillers before energizing the switchboard. Refer to Table 4 and Table 5 for sizes and catalog numbers.
Failure to follow these instructions will result in death or serious injury.

QMB/QMJ Fusible Switch Blank Fillers

Height

Catalog No.

1.50 in. (38 mm)

QMB1BLW

3.00 in. (76 mm)

QMB3BLW

6.00 in. (152 mm)

QMB6BLW

15.00 in. (381 mm)

QMB15BLW

QMQB* Fusible Switch Blank Fillers

Height

Catalog No.

2x: 1.375 in. (35 mm)

QFS1

8x: 5.50 in. (140 mm)

QFS5

10x: 6.875 in. (175 mm)

QFS6

14x: 9.625 in. (244 mm)

QFS9

24x: 16.50 in. (419 mm)

QFS16

NOTICE
Plug-On Connector DAMAGE
Do not remove the protective lubricant on the plug-on connectors.
Failure to follow these instructions can result in equipment damage.
  1. Turn off the main power.

  2. Turn the switch handle(s) to the OFF position. Align switch plug-on connectors with QMB panel vertical bus, and plug switch onto panel.

  3. Place and partially tighten all unit mounting screws that mount to the QMB panel mounting rails.

  4. Tighten all screws evenly. The unit mounting flange and plug-on connectors must be seated securely.

Removing QMB/QMJ/QMQB Fusible Switches

NOTE: QMQB switches are available in Canada only.
  1. Turn off the main power.

  2. Turn switch handle(s) to the OFF position.

  3. Disconnect the load wires.

  4. For QMB and QMJ switches, remove mounting screws holding the switch to the mounting rail. For QMQB* switches, remove the bolts holding the switch to the line terminal.

  5. Unplug the switch.

Ground Fault Protection Systems

Check the terminal connections on the ground fault protection system at least once a year for tightness and corrosion. If the system can be tested without tripping the main or branch device, directions for testing the system are in the device manual. Otherwise, testing the ground fault protection system trips the main or branch device to which it is connected. If the ground fault sensor or relay is physically or electrically damaged, replace it.

If the ground fault protection system does not operate properly and additional equipment has been connected to the installation since the last maintenance test/check, de-energize the entire system, and check for grounds on the neutral downstream from the main bonding jumper. If no downstream grounds are detected and the ground fault system is not operating properly, contact Schneider Electric Services at 1-888-778-2733 (US) or 1-800-565-6699 (Canada).

If no additions have been made to the installation and the ground fault protection system does not operate properly, contact Schneider Electric Services at 1-888-778-2733 (US) or 1-800-565-6699 (Canada).

Refer to the ground fault field test instruction manual for additional testing information. If the manual is not available, refer to Reference Publications to obtain the appropriate number. Contact your local Schneider Electric representative to obtain this manual.

Continuous Thermal Monitoring (CTM) Sensors

Refer to the Schneider Electric thermal monitoring sensors instruction manuals shipped with the switchboard for complete installation and maintenance information. If the instruction manuals are not available, refer to Reference Publications for the appropriate number, or contact your local Schneider Electric representative.

Sensor Maintenance

Only qualified electrical personnel can service Continuous Thermal Monitoring sensors.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.