Antenna Installation

You have just received your new PrismaSeT Active switchboard.

Discover in the following video how easy it is to install the LoRa antenna on top of your switchboard.

Steps to Install the LoRa Antenna on PrismaSeT G Active

  1. Remove the cable gland plate. The antenna can be found under the metal cover on the left side of the switchboard.

  2. Take out the antenna.

  3. Insert the antenna cable in the dedicated slot of the metal cover.

    NOTE: Be careful not to twist the cable too much (R < 50 mm).
  4. Install the cable gland plate back.

  5. Place the antenna on the magnetic part on the left side of the switchboard. The metallic bracket that is provided can also be used to place the antenna in a better location.

    NOTE: The antenna must always be placed vertically.

Steps to Install the LoRa Antenna on PrismaSeT P Active

  1. The antenna is delivered with the lateral panels, the Wireless Panel Server and the wiring kit.

  2. Unpack the antenna from its packaging.

  3. Connect the antenna to the Wireless Panel Server using the small gap on top of the green bar.

    NOTE: Tighten by hand only.
  4. Place the antenna on top of your panel at the desired location. The metallic bracket that is provided can also be used to place the antenna in a better location.

    NOTE: The antenna must always be placed vertically.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.