DOCA0224EN-11

Configuration Software

Following are the compatible software and DTM library required to configure and use the TeSys island module:

  • SoMove software v2.9.7 or later

  • EcoStruxure Control Expert v15.0 SP1 or later

  • TeSys island DTM Library v1.0.1401 or later

  • EcoStruxure Automation Expert - Motion v24.1.0.0

  • EcoStruxure Machine Expert v1.1 or later

  • TIA portal v15 or later

  • RS5000 v30 or later

NOTE: For software configuration, refer to the compatibility table in section Compatibility

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.