DOCA0224EN-11

Version 003.003.000

New Features

IO Optimization feature extension to EcoStruxure Control Expert and EcoStruxure Automation Expert-Motion function blocks library.

Bugs Fixed

  • Incorrect asset data (running hours) is displayed in SoMove and Operation and maintenance tool after firmware upgrade.

  • When a firmware upgrade or downgrade occurs, the correct firmware version information is not updated in the audit log.

Known Issues

The function blocks (system energy basic, system power basic, and system voltage enhanced) reset pins are failing to execute for EcoStruxure Automation Expert-Motion.

Workaround: Energy parameters can be reset using DTM interface under system avatar's Energy Monitoring view.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.