DOCA0224EN-11

TeSys island Overview

TeSys island delivers a connected and customized system for the direct control and management of low-voltage loads. The TeSys island optimizes availability of the physical modules with embedded pre-alarming management capabilities.

TeSys island targets performance and high performance machines with automation architectures based on high-speed networks connecting devices to a PLC. Machinery operating at high production rates must avoid unplanned production downtime, which can be extremely costly. TeSys island helps to reduce unplanned downtime with predictive maintenance so that repairs can be completed during a scheduled maintenance window.

TeSys island is fully integrated into the PLC programming environment using digital objects. TeSys island is fully integrated into the EcoStruxure portfolio that combines products and software packages into automation solutions for OEMs and machine builders. The system also supports integration into third-party PLC.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.