Compatibility
The following table shows the compatibility of digital tools with TeSys island module in active releases.
|
Configuration/Programming software |
TeSys island firmware version |
||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|
|
TeSysisland_001.100.0013.sedp |
TeSysisland_002.100.016.sedp |
TeSysisland_002.200.008.sedp |
TeSysisland_002.300.006.sedp |
TeSysisland_003.000.002.sedp |
TeSysisland_003.001.001.sedp |
TeSysisland_003.002.000.sedp |
TeSysisland_003.003.000.sedp |
TeSysisland_003.003.001.sedp |
TeSysisland_003.003.005.sedp |
||
|
DTM (SoMove or any FDT container) |
DTM v1.0.1401 |
✔ |
X |
X |
X |
X |
X |
X |
X |
X |
X |
|
DTM v1.1.0 |
✔ |
X |
X |
X |
X |
X |
X |
X |
X |
X |
|
|
DTM v2.1.1 |
✔ |
✔ |
X |
X |
X |
X |
X |
X |
X |
X |
|
|
NOTE: DTM v2.1.1 is compatible when using Modbus TCP or EtherNet/IP and
for previously existing device and load avatars only.
|
|||||||||||
|
DTM v2.2.0 or DTM v2.2.1 (equivalent) |
X |
X |
✔ |
✔ |
X |
X |
X |
X |
X |
X |
|
|
DTM v2.3.0 |
X |
X |
X |
✔ |
X |
X |
X |
X |
X |
X |
|
|
DTM v2.4.0 |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
|
|
DTM v2.4.1 |
X |
X |
X |
X |
✔ |
✔ |
X |
X |
X |
X |
|
|
DTM v2.4.2 |
X |
X |
X |
X |
X |
✔ |
X |
X |
X |
X |
|
|
DTM v2.4.3 |
X |
X |
X |
X |
X |
X |
✔ |
X |
X |
X |
|
|
DTM v2.4.4 |
X |
X |
X |
X |
X |
X |
✔ |
X |
X |
X |
|
|
DTM v3.0.0 |
X |
X |
X |
X |
X |
X |
X |
✔ |
✔ |
X |
|
|
DTM v3.0.1 |
X |
X |
X |
X |
X |
X |
X |
✔ |
✔ |
X |
|
|
DTM v3.0.2 |
X |
X |
X |
X |
X |
X |
X |
X |
X |
✔ |
|
|
EcoStruxure Machine Expert |
EcoStruxure Machine Expert v1.1 or v1.2 Function block library: 1.0.15.0 Device description:
|
✔ |
X |
X |
X |
X |
X |
X |
X |
X |
X |
|
EcoStruxure Machine Expert v1.2.3 or later Function block library: 2.0.2.0 Device description:
|
X |
X |
✔ |
✔ |
**✔ |
**✔ |
X |
X |
X |
X |
|
|
EcoStruxure Machine Expert v2.2.2 Function block library: 3.0.0.0 Device description:
|
X |
X |
X |
X |
X |
X |
*✔ |
X |
X |
X |
|
|
EcoStruxure Machine Expert v2.3 Function block library: 4.0.6.0 Device description:
|
X |
X |
X |
X |
X |
X |
X |
X |
✔ |
***✔ |
|
|
@New D1
EcoStruxure Machine Expert v2.6 |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
|
|
NOTE:
Workaround: Use the Schneider Electric Machine Expert Modbus TCP PLCs as a third party PLC. |
|||||||||||
|
EcoStruxure Automation Expert-Motion |
EcoStruxure Automation Expert-Motion vM_24.1.0.0 Function block library: 4.0.5.0 Device description:
|
X |
X |
X |
X |
X |
X |
X |
✔ |
✔ |
*✔ |
|
NOTE: *All new parameters (ATEX configuration
status and minor event status for all avatars) will be not be available
in Control Function Blocks.
|
|||||||||||
|
EcoStruxure Control Expert V15.0 SP1 |
EcoStruxure Control Expert–TeSys island Library PSx DTM Library v3.14.54 PLC M580 - CPU firmware 3.20 |
X |
X |
✔ |
✔ |
*✔ |
*✔ |
*✔ |
X |
X |
X |
|
NOTE: *EcoStruxure Control Expert is
not compatible, if there is change in the .
|
|||||||||||
|
EcoStruxure Control Expert V16.0 or later |
EcoStruxure Control Expert–TeSys island Library v2.2 PSx DTM Library v3.19.24107 PLC M580 - CPU firmware 3.20 |
X |
X |
X |
X |
X |
X |
X |
✔ |
✔ |
*✔ |
|
NOTE: *All new parameters (ATEX configuration
status and minor event status for all avatars) will be not be available
in Control Function Blocks.
|
|||||||||||
|
Studio 5000 V30 or later |
NA |
NA |
NA |
✔ |
✔ |
*✔ |
*✔ |
*✔ |
X |
X |
X |
|
NOTE: Ensure that the export of L5X file
is done with the compatible version of DTM.
NOTE: *When PIM
with IO avatar is used with TeSys island, then the function blocks are not compatible with RS5000.
|
|||||||||||
|
TIA Portal V15 or later |
Library: TeSysisland_TIAV15_V2.1.1.zal15 GSD: SCHE1135.GSD (revision 1.0) GSDML: GSDML-V2.35-SchneiderElectric-TeSysisland-20200202.xml NOTE: Ensure that the export of AML file is done with the compatible
version of DTM.
|
X |
✔ |
X |
X |
X |
X |
X |
X |
X |
X |
|
Library: TeSysIsland_TIAV15_V2.2.0.zal15 GSD: SCHE1135.GSD (revision 2.0) GSDML: GSDML-V2.35-SchneiderElectric-TeSysisland-20200404.xml NOTE: Ensure that the export of AML file is done with the compatible
version of DTM.
|
X |
X |
✔ |
✔ |
*✔ |
*✔ |
*✔ |
X |
X |
X |
|
|
NOTE: *When PIM with IO avatar is used
with TeSys island, then the function blocks are not compatible with TIA portal.
|
|||||||||||