DOCA0260EN-00

Date and Time

To avoid errors, it is important to keep the date and time synchronized.

The following procedure shows how to update the date and time settings for Ethernet interface modules using standard web server or TeSys Tera DTM:

  1. Navigate to Settings > General > Date & Time.

  2. Using the Date & Time Selection drop-down list, select one of the following options:

    • Manual

      NOTE:
      • When the date and time are set manually, the LTMT main unit resets to factory settings upon reboot.

      • The date and time settings can be update manually using the TeSys Tera DTM or the LTMTCUF control operator unit.

    • NTP

      NOTE: NTP protocol is available only for the Ethernet versions of the LTMT main unit.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?