DOCA0260EN-00

Introduction

Cybersecurity as part of Process, Tools and Technology, Compliance, and Governance, aims at safeguarding your communication network and all connected devices from attacks that could disrupt operations (availability), alter information (integrity), or expose confidential data (confidentiality).

The objective of cybersecurity is to provide increased levels of protection for information and physical assets from theft, corruption, misuse, or accidents while maintaining access for their intended users. There are many aspects to cybersecurity including designing secure systems, restricting access using physical and digital methods, identifying users, as well as implementing security control/measurement procedures and best practice policies.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?